Function | File |
---|---|
driver | sound/soc/codecs/ssm4567.c |
include | sound/soc/codecs/ssm4567.h |
For compile time configuration, it’s common Linux practice to keep board- and application-specific configuration out of the main driver file, instead putting it into the board support file.
For devices on custom boards, as typical of embedded and SoC-(system-on-chip) based hardware, Linux uses platform_data to point to board-specific structures describing devices and how they are connected to the SoC. This can include available ports, chip variants, preferred modes, default initialization, additional pin roles, and so on. This shrinks the board-support packages (BSPs) and minimizes board and application specific #ifdefs in drivers.
Unlike PCI or USB devices, I2C devices are not enumerated at the hardware level. Instead, the software must know which devices are connected on each I2C bus segment, and what address these devices are using. For this reason, the kernel code must instantiate I2C devices explicitly. There are different ways to achieve this, depending on the context and requirements. However the most common method is to declare the I2C devices by bus number.
This method is appropriate when the I2C bus is a system bus, as in many embedded systems, wherein each I2C bus has a number which is known in advance. It is thus possible to pre-declare the I2C devices that inhabit this bus. This is done with an array of struct i2c_board_info, which is registered by calling i2c_register_board_info().
So, to enable such a driver one need only edit the board support file by adding an appropriate entry to i2c_board_info.
For more information see: Documentation/i2c/instantiating-devices.rst
The I2C address of the SSM4567 depends on the setting of the ADDR pin.
ADDR | I2C Address |
---|---|
0 | 0x34 |
1 | 0x35 |
static struct i2c_board_info __initdata bfin_i2c_board_info[] = {
[--snip--]
{
I2C_BOARD_INFO("ssm4567", 0x34),
},
[--snip--]
}
static int __init stamp_init(void)
{
[--snip--]
i2c_register_board_info(0, bfin_i2c_board_info,
ARRAY_SIZE(bfin_i2c_board_info));
[--snip--]
return 0;
}
arch_initcall(board_init);
i2s: i2c@41600000 {
compatible = "...;
...
#size-cells = <0>;
#address-cells = <1>;
ssm4567: ssm4567@34 {
compatible = "adi,ssm4567";
reg = <0x34>;
};
};
Name | Description |
---|---|
OUT | Class-D Amplifier Output |
Name | Description |
---|---|
DAC High Pass Filter Switch | Enables/Disables the high-pass filter for the DAC |
DAC Low Power Switch | Enables/Disables low-power mode of the DAC |
Master Playback Volume | Digital output volume control. |
Low-EMI Switch | Enables/Disables low EMI mode. |
Limiter Mode | Mode the output limiter is using. |
Limiter Attack Rate | Attack rate of the output limiter. |
Limiter Release Rate | Release rate of the output limiter. |
Limiter Attack Threshold | Attack threshold for the output limiter. |
Amplifier Boost Switch | Enables/Disables the output amplifier booster |
The amplifier driver registers one DAIs, one for each serial port. The DAI is named “ssm4567-hifi”
Name | Supported by driver | Description |
---|---|---|
SND_SOC_DAIFMT_I2S | yes | I2S mode |
SND_SOC_DAIFMT_RIGHT_J | no | Right Justified mode |
SND_SOC_DAIFMT_LEFT_J | yes | Left Justified mode |
SND_SOC_DAIFMT_DSP_A | yes | data MSB after FRM LRC |
SND_SOC_DAIFMT_DSP_B | yes | data MSB during FRM LRC |
SND_SOC_DAIFMT_AC97 | no | AC97 mode |
SND_SOC_DAIFMT_PDM | yes | Pulse density modulation |
SND_SOC_DAIFMT_NB_NF | yes | Normal bit- and frameclock |
SND_SOC_DAIFMT_NB_IF | yes | Normal bitclock, inverted frameclock |
SND_SOC_DAIFMT_IB_NF | yes | Inverted frameclock, normal bitclock |
SND_SOC_DAIFMT_IB_IF | yes | Inverted bit- and frameclock |
SND_SOC_DAIFMT_CBM_CFM | no | Codec bit- and frameclock master |
SND_SOC_DAIFMT_CBS_CFM | no | Codec bitclock slave, frameclock master |
SND_SOC_DAIFMT_CBM_CFS | no | Codec bitclock master, frameclock slave |
SND_SOC_DAIFMT_CBS_CFS | yes | Codec bit- and frameclock slave |
If you want to use the SSM4567 in TDM mode you can configure it using snd_soc_dai_set_tdm_slot() from you ASoC board driver.
The following restrictions apply to the parameters of snd_soc_dai_set_tdm_slot().
Example:
static int ssm4567_link_init(struct snd_soc_pcm_runtime *rtd)
{
int ret;
ret = snd_soc_dai_set_tdm_slot(rtd->codec_dai, 0x01, 0x01, 8, 32);
if (ret < 0)
return ret;
return 0;
}
static struct snd_soc_dai_link ssm4567_dai_link = {
...,
.init = ssm4567_link_init,
};
static const struct snd_soc_dapm_widget ssm4567_zed_widgets[] = {
SND_SOC_DAPM_SPK("Speaker", NULL),
};
static const struct snd_soc_dapm_route ssm4567_zed_routes[] = {
{ "Speaker", NULL, "OUT" },
};
static struct snd_soc_dai_link ssm4567_zed_dai_link = {
.name = "ssm4567",
.stream_name = "ssm4567",
.codec_dai_name = "ssm4567-hifi",
.dai_fmt = SND_SOC_DAIFMT_DSP_A |
SND_SOC_DAIFMT_NB_NF |
SND_SOC_DAIFMT_CBS_CFS,
.init = ssm4567_zed_init,
};
static struct snd_soc_card ssm4567_zed_card = {
.name = "ZED SSM4567",
.owner = THIS_MODULE,
.dai_link = &zed_ssm4567_dai_link,
.num_links = 1,
.dapm_widgets = zed_ssm4567_widgets,
.num_dapm_widgets = ARRAY_SIZE(zed_ssm4567_widgets),
.dapm_routes = zed_ssm4567_routes,
.num_dapm_routes = ARRAY_SIZE(zed_ssm4567_routes),
.fully_routed = true,
};
This example shows how to setup a ASoC board driver for a system with two SSM4567, one driving the left speaker and the other driving the right speaker. In this example the left SSM4567 is at I2C address 0x34 (ADDR=0) and the right SSM4567 is at I2S address 0x35 (ADDR=1).
Note support for multiple CODECs on a single DAI link requires Linux v3.17 or higher.
static int ssm4567_link_init(struct snd_soc_pcm_runtime *rtd)
{
int ret;
/* Slot 0 for left */
ret = snd_soc_dai_set_tdm_slot(rtd->codec_dais[0], 0x01, 0x01, 2, 32);
if (ret < 0)
return ret;
/* Slot 2 for right */
ret = snd_soc_dai_set_tdm_slot(rtd->codec_dais[1], 0x02, 0x02, 2, 32);
if (ret < 0)
return ret;
return 0;
}
static const struct snd_soc_dapm_widget ssm4567_zed_widgets[] = {
SND_SOC_DAPM_SPK("Left Speaker", NULL),
SND_SOC_DAPM_SPK("Right Speaker", NULL),
};
static const struct snd_soc_dapm_route ssm4567_zed_routes[] = {
{ "Left Speaker", NULL, "Left OUT" },
{ "Right Speaker", NULL, "Right OUT" },
};
static const snd_soc_dai_link_component ssm4567_zed_codec_components[] = {
{ /* Left */
.name = "ssm4567.0-0034",
.codec_dai_name = "ssm4567-hifi",
},
{ /* Right */
.name = "ssm4567.0-0035",
.codec_dai_name = "ssm4567-hifi",
},
};
/* Assign prefix to avoid name conflicts */
static const struct snd_soc_codec_conf ssm4567_zed_codec_conf[] = {
{
.dev_name = "ssm4567.0-0034",
.name_prefix = "Left",
},
{
.dev_name = "ssm4567.0-0035",
.name_prefix = "Right",
},
};
static struct snd_soc_dai_link ssm4567_zed_dai_link = {
.name = "ssm4567",
.stream_name = "ssm4567",
.codecs = ssm4567_zed_codec_components,
.num_codecs = ARRAY_SIZE(ssm4567_zed_codec_components),
.codec_conf = ssm4567_zed_codec_conf,
.num_configs = ARRAY_SIZE(ssm4567_zed_codec_conf),
.dai_fmt = SND_SOC_DAIFMT_DSP_A |
SND_SOC_DAIFMT_NB_NF |
SND_SOC_DAIFMT_CBS_CFS,
.init = ssm4567_link_init,
};
static struct snd_soc_card ssm4567_zed_card = {
.name = "ZED SSM4567",
.owner = THIS_MODULE,
.dai_link = &zed_ssm4567_dai_link,
.num_links = 1,
.dapm_widgets = zed_ssm4567_widgets,
.num_dapm_widgets = ARRAY_SIZE(zed_ssm4567_widgets),
.dapm_routes = zed_ssm4567_routes,
.num_dapm_routes = ARRAY_SIZE(zed_ssm4567_routes),
.fully_routed = true,
};