This is a Linux industrial I/O (IIO) subsystem driver, targeting serial interface Inertial Measurement Units (IMU). The industrial I/O subsystem provides a unified framework for drivers for many different types of converters and sensors using a number of different physical interfaces (i2c, spi, etc). See IIO for more information.
Function | File |
---|---|
driver | drivers/iio/imu/adis16475.c |
Analog Devices ADIS16475 and similar IMUs
compatible: Must be one of
reg: SPI chip select number for the device
imu@0 {
compatible = "adi,adis16475-3";
reg = <0>;
spi-cpha;
spi-cpol;
spi-max-frequency = <2000000>;
interrupts = <4 IRQ_TYPE_EDGE_RISING>;
interrupt-parent = <&gpio>;
};
For more supported devicetree properties take a look to dt-bindings.
Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)
The adis16475 driver depends on CONFIG_SPI_MASTER
Linux Kernel Configuration
Device Drivers --->
<*> Industrial I/O support --->
--- Industrial I/O support
[*] Enable buffer support within IIO
-*- Industrial I/O buffering based on kfifo
-*- Enable triggered sampling support
[--snip--]
Inertial measurement units --->
[--snip--]
<*> Analog Devices ADIS16475 and similar IMU driver
[--snip--]
The evaluation kits simplify the process of connecting an IMU to an embedded processor system using a 16-pin, 1mm ribbon cable. For a detailed description check the links (on the beginning of the page) for the appropriated evaluation kit. Here is an example of basic connection from one ADIS device interface connector to the host:(microprocessor):
DEVICE HOST MICROPROCESSOR
* DR ———————> IRQ GPIO
* CS <——————— SPI_SEL
* SCLK <——————— SPI_SCLK
* DIN <——————— SPI_MOSI
* DOUT ———————> SPI_MISO
Each and every IIO device, typically a hardware chip, has a device folder under /sys/bus/iio/devices/iio:deviceX. Where X is the IIO index of the device. Under every of these directory folders reside a set of files, depending on the characteristics and features of the hardware device in question. These files are consistently generalized and documented in the IIO ABI documentation. In order to determine which IIO deviceX corresponds to which hardware device, the user can read the name file /sys/bus/iio/devices/iio:deviceX/name. In case the sequence in which the iio device drivers are loaded/registered is constant, the numbering is constant and may be known in advance.
TIP: An example program which uses the interface can be found here:
This specifies any shell prompt running on the target
root:/> **cd /sys/bus/iio/devices/**
root:/sys/bus/iio/devices> **ls**
iio:device0 trigger0
root:/sys/bus/iio/devices> **cd iio:device0**
root:/sys/bus/iio/devices/iio:device0> **ls -l**
total 0
drwxr-xr-x 2 root root 0 Jul 12 10:17 buffer
-rw-r--r-- 1 root root 4096 Jul 12 10:17 current_timestamp_clock
-r--r--r-- 1 root root 4096 Jul 12 10:17 dev
-rw-r--r-- 1 root root 4096 Jul 12 10:17 filter_low_pass_3db_frequency
-rw-r--r-- 1 root root 4096 Jul 12 10:17 in_accel_scale
-rw-r--r-- 1 root root 4096 Jul 12 10:17 in_accel_x_calibbias
-rw-r--r-- 1 root root 4096 Jul 12 10:17 in_accel_x_raw
-rw-r--r-- 1 root root 4096 Jul 12 10:17 in_accel_y_calibbias
-rw-r--r-- 1 root root 4096 Jul 12 10:17 in_accel_y_raw
-rw-r--r-- 1 root root 4096 Jul 12 10:17 in_accel_z_calibbias
-rw-r--r-- 1 root root 4096 Jul 12 10:17 in_accel_z_raw
-rw-r--r-- 1 root root 4096 Jul 12 10:17 in_anglvel_scale
-rw-r--r-- 1 root root 4096 Jul 12 10:17 in_anglvel_x_calibbias
-rw-r--r-- 1 root root 4096 Jul 12 10:17 in_anglvel_x_raw
-rw-r--r-- 1 root root 4096 Jul 12 10:17 in_anglvel_y_calibbias
-rw-r--r-- 1 root root 4096 Jul 12 10:17 in_anglvel_y_raw
-rw-r--r-- 1 root root 4096 Jul 12 10:17 in_anglvel_z_calibbias
-rw-r--r-- 1 root root 4096 Jul 12 10:17 in_anglvel_z_raw
-rw-r--r-- 1 root root 4096 Jul 12 10:17 in_temp0_raw
-rw-r--r-- 1 root root 4096 Jul 12 10:17 in_temp0_scale
-r--r--r-- 1 root root 4096 Jul 12 10:17 name
lrwxrwxrwx 1 root root 0 Jul 12 10:17 of_node -> ../../../../../../../../firmware/devicetree/base/soc/spi@7e204000/adis16475@0
drwxr-xr-x 2 root root 0 Jul 12 10:17 power
-rw-r--r-- 1 root root 4096 Jul 12 10:17 sampling_frequency
drwxr-xr-x 2 root root 0 Jul 12 10:17 scan_elements
lrwxrwxrwx 1 root root 0 Jul 12 10:17 subsystem -> ../../../../../../../../bus/iio
drwxr-xr-x 2 root root 0 Jul 12 10:17 trigger
-rw-r--r-- 1 root root 4096 Jul 12 10:17 uevent
root:/sys/bus/iio/devices/iio:device0>
For a detailed description please see: Documentation/ABI/testing/sysfs-bus-iio
3-Axis Accelerometer related device files | Description |
---|---|
in_accel_scale | Scale for the accelerometer channels. |
in_accel_x_calibbias | Calibration offset for the X-axis accelerometer channel. |
in_accel_x_raw | Raw X-axis accelerometer channel value. |
in_accel_y_calibbias | Calibration offset for the Y-axis accelerometer channel. |
in_accel_y_raw | Raw Y-axis accelerometer channel value. |
in_accel_z_calibbias | Calibration offset for the Z-axis accelerometer channel. |
in_accel_z_raw | Raw Z-axis accelerometer channel value. |
3-Axis Gyro related device files | Description |
in_anglvel_scale | Scale for the gyroscope channels. |
in_anglvel_x_calibbias | Calibration offset for the X-axis gyroscope channel. |
in_anglvel_x_raw | Raw X-axis gyroscope channel value. |
in_anglvel_y_calibbias | Calibration offset for the Y-axis gyroscope channel. |
in_anglvel_y_raw | Raw Y-axis gyroscope channel value. |
in_anglvel_z_calibbias | Calibration offset for the Z-axis gyroscope channel. |
in_anglvel_z_raw | Raw Z-axis gyroscope channel value. |
Temperature sensor related files | Description |
in_temp0_raw | Raw temperature channel value. |
in_temp0_scale | Scale for the temperature sensor channel. |
Miscellaneous device files | Description |
name | Name of the IIO device. |
sampling_frequency | Currently selected sample rate. |
filter_low_pass_3db_frequency | Bandwidth for the accelerometer and gyroscope channels. |
burst_mode_enable | Enables reading of the data with a SPI burst read. |
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device0> **cat name**
adis16477-1
The sampling frequency of the device can be set by writing the desired value to the sampling_frequency
file. The driver will automatically round up to the nearest supported sampling frequency.
Example:
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device0> **cat sampling_frequency**
2000.000000
pi@raspberrypi:/s
root:/sys/bus/iio/devices/iio:device0> **echo 1000 > sampling_frequency**
root:/sys/bus/iio/devices/iio:device0> **cat sampling_frequency**
1000.000000
A channel value can be read from its _raw
attribute. The value returned by the _raw
attribute is the raw value as reported by the device. To get the processed value of the channel in a standardized unit add the channels _offset
attribute to the _raw
value and multiply the result by _scale
attribute. If no _offset
attribute is present assume 0 for the offset.
processed value = (raw + offset) * scale
The units by the IIO framework are:
Example:
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device0> **cat in_accel_z_raw**
52612913
root:/sys/bus/iio/devices/iio:device0> **cat in_accel_scale**
0.000000187
Z-axis acceleration = in_accel_z_raw * in_accel_scale = 52612913 * 0.000000187 m/s^2 = 9.838 m/s^2
The gyro and accel bandwidth can be set by writing the desired value to the filter_low_pass_3db_frequency
attribute. The driver will automatically round up to the nearest supported bandwidth.
Example:
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device0> **cat filter_low_pass_3db_frequency**
720.000000
root:/sys/bus/iio/devices/iio:device0> **echo 360 > filter_low_pass_3db_frequency**
root:/sys/bus/iio/devices/iio:device0> **cat filter_low_pass_3db_frequency**
360.000000
This driver only supports it's own default trigger source adis16477-1-dev0
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device0> **cat trigger/current_trigger**
adis16477-1-dev0
In case there is no trigger specified, run the following command:
root@analog:/sys/bus/iio/devices# **cat trigger0/name > iio\:device0/trigger/current_trigger**
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device0/buffer> **ls**
**data_available** **enable** **length** **watermark**
The Industrial I/O subsystem provides support for various ring buffer based data acquisition methods. Apart from device specific hardware buffer support, the user can chose between two different software ring buffer implementations. One is the IIO lock free software ring, and the other is based on Linux kfifo. Devices with buffer support feature an additional sub-folder in the /sys/bus/iio/devices/deviceX/ folder hierarchy. Called deviceX:bufferY, where Y defaults to 0, for devices with a single buffer.
Every buffer implementation features a set of files:
length
Get/set the number of sample sets that may be held by the buffer.
enable
Enables/disables the buffer. This file should be written last, after length and selection of scan elements.
watermark
A single positive integer specifying the maximum number of scan elements to wait for. Poll will block until the watermark is reached. Blocking read will wait until the minimum between the requested read amount or the low water mark is available. Non-blocking read will retrieve the available samples from the buffer even if there are less samples then watermark level. This allows the application to block on poll with a timeout and read the available samples after the timeout expires and thus have a maximum delay guarantee.
data_available
A read-only value indicating the bytes of data available in the buffer. In the case of an output buffer, this indicates the amount of empty space available to write data to. In the case of an input buffer, this indicates the amount of data available for reading.
length_align_bytes
Using the high-speed interface. DMA buffers may have an alignment requirement for the buffer length.
Newer versions of the kernel will report the alignment requirements
associated with a device through the length_align_bytes
property.
scan_elements
The scan_elements directory contains interfaces for elements that will be captured for a single triggered sample set in the buffer.
This specifies any shell prompt running on the target
root:/sys/bus/iio/devices/iio:device0/scan_elements> **ls -l**
total 0
-rw-r--r-- 1 root root 4096 Jul 12 10:17 in_accel_x_en
-r--r--r-- 1 root root 4096 Jul 12 10:17 in_accel_x_index
-r--r--r-- 1 root root 4096 Jul 12 10:17 in_accel_x_type
-rw-r--r-- 1 root root 4096 Jul 12 10:17 in_accel_y_en
-r--r--r-- 1 root root 4096 Jul 12 10:17 in_accel_y_index
-r--r--r-- 1 root root 4096 Jul 12 10:17 in_accel_y_type
-rw-r--r-- 1 root root 4096 Jul 12 10:17 in_accel_z_en
-r--r--r-- 1 root root 4096 Jul 12 10:17 in_accel_z_index
-r--r--r-- 1 root root 4096 Jul 12 10:17 in_accel_z_type
-rw-r--r-- 1 root root 4096 Jul 12 10:17 in_anglvel_x_en
-r--r--r-- 1 root root 4096 Jul 12 10:17 in_anglvel_x_index
-r--r--r-- 1 root root 4096 Jul 12 10:17 in_anglvel_x_type
-rw-r--r-- 1 root root 4096 Jul 12 10:17 in_anglvel_y_en
-r--r--r-- 1 root root 4096 Jul 12 10:17 in_anglvel_y_index
-r--r--r-- 1 root root 4096 Jul 12 10:17 in_anglvel_y_type
-rw-r--r-- 1 root root 4096 Jul 12 10:17 in_anglvel_z_en
-r--r--r-- 1 root root 4096 Jul 12 10:17 in_anglvel_z_index
-r--r--r-- 1 root root 4096 Jul 12 10:17 in_anglvel_z_type
-rw-r--r-- 1 root root 4096 Jul 12 10:17 in_flags0_en
-r--r--r-- 1 root root 4096 Jul 12 10:17 in_flags0_index
-r--r--r-- 1 root root 4096 Jul 12 10:17 in_flags0_type
-rw-r--r-- 1 root root 4096 Jul 12 10:17 in_flags1_crc_en
-r--r--r-- 1 root root 4096 Jul 12 10:17 in_flags1_crc_index
-r--r--r-- 1 root root 4096 Jul 12 10:17 in_flags1_crc_type
-rw-r--r-- 1 root root 4096 Jul 12 10:17 in_temp0_en
-r--r--r-- 1 root root 4096 Jul 12 10:17 in_temp0_index
-r--r--r-- 1 root root 4096 Jul 12 10:17 in_temp0_type
-rw-r--r-- 1 root root 4096 Jul 12 10:17 in_timestamp_en
-r--r--r-- 1 root root 4096 Jul 12 10:17 in_timestamp_index
-r--r--r-- 1 root root 4096 Jul 12 10:17 in_timestamp_type
root:/sys/bus/iio/devices/iio:device0/scan_elements>
From the above list, note the following 2 elements:
Both this elements are relevant only when burst_mode_enable is set
in_voltageX_en / in_voltageX-voltageY_en / timestamp_en:
Scan element control for triggered data capture. Writing 1 will enable the scan element, writing 0 will disable it
in_voltageX_type / in_voltageX-voltageY_type / timestamp_type:
Description of the scan element data storage within the buffer and therefore in the form in which it is read from user-space. Form is [s|u]bits/storage-bits. s or u specifies if signed (2's complement) or unsigned. bits is the number of bits of data and storage-bits is the space (after padding) that it occupies in the buffer. Note that some devices will have additional information in the unused bits so to get a clean value, the bits value must be used to mask the buffer output value appropriately. The storage-bits value also specifies the data alignment. So u12/16 will be a unsigned 12 bit integer stored in a 16 bit location aligned to a 16 bit boundary. For other storage combinations this attribute will be extended appropriately.
in_voltageX_index / in_voltageX-voltageY_index / timestamp_index:
A single positive integer specifying the position of this scan element in the buffer. Note these are not dependent on what is enabled and may not be contiguous. Thus for user-space to establish the full layout these must be used in conjunction with all _en attributes to establish which channels are present, and the relevant _type attributes to establish the data storage format.
Setting up the driver on the official Raspbian image.
Resources:
Properties | ADIS16475 | ADIS16480 |
---|---|---|
Supported sensors | adis16470, adis16475-1, adis16475-2, adis16475-3, adis16477-1, adis16477-2, adis16477-3, adis16465-1, adis16465-2, adis16465-3, adis16467-1, adis16467-2, adis16467-3, adis16500, adis16505-1, adis16505-2, adis16505-3, adis16507-1, adis16507-2, adis16507-3 | adis16375, adis16480, adis16485, adis16488, adis16490, adis16495-1, adis16495-2, adis16495-3, adis16497-1, adis16497-2, adis16497-3 |
Required overlays | adis16475-overlays.dts | adis16480-overlays.dts |
Overlay contents:
adis16475-overlay.dts | adis16480-overlay.dts |
---|---|
// SPDX-License-Identifier: GPL-2.0 /dts-v1/; /plugin/; #include <dt-bindings/interrupt-controller/irq.h> #include <dt-bindings/gpio/gpio.h> / { compatible = "brcm,bcm2835"; fragment@0 { target = <&spi0>; __overlay__ { status = "okay"; }; }; fragment@1 { target = <&spidev0>; __overlay__ { status = "disabled"; }; }; fragment@2 { target = <&spidev1>; __overlay__ { status = "disabled"; }; }; fragment@3 { target = <&gpio>; __overlay__ { adis16475_pins: adis16475_pins { brcm,pins = <4 12>; // interrupt and reset brcm,function = <0 1>; // in out }; }; }; fragment@4 { target-path = "/"; __overlay__ { clocks { adis16475_ref_clk: [clock](http://www.opengroup.org/onlinepubs/009695399/functions/clock.html)@0 { #clock-cells = <0>; compatible = "fixed-clock"; }; }; }; }; fragment@5 { target = <&spi0>; __overlay__ { /* needed to avoid dtc warning */ #address-cells = <1>; #size-cells = <0>; adis16475: adis16475@0 { reg = <0>; pinctrl-names = "default"; pinctrl-0 = <&adis16475_pins>; spi-cpha; spi-cpol; reset-gpios = <&gpio 12 GPIO_ACTIVE_LOW>; spi-max-frequency = <2000000>; interrupts = <4 IRQ_TYPE_EDGE_RISING>; interrupt-parent = <&gpio>; }; }; }; __overrides__ { /* * This gives an option to use the gpio25 as the data ready pin. This * must be used for the adis16465/7 families as these devices use the * 14 pin connector where DR is using gpio25. Note that this should * not be used for the other devices as the gpio25 is both connected to * the sync selector and to the sync pin (because the sync and DR pins * are swapped in the 16 pin connector). */ drdy_gpio25 = <&adis16475_pins>,"brcm,pins:0=25", <&adis16475>,"interrupts:0=25"; device = <&adis16475>,"compatible"; sync_mode = <&adis16475>,"adi,sync-mode:0"; ext_sync_freq = <&adis16475_ref_clk>, "clock-frequency:0", <&adis16475>,"clocks:0=",<&adis16475_ref_clk>; }; }; |
// SPDX-License-Identifier: GPL-2.0 /dts-v1/; /plugin/; #include <dt-bindings/interrupt-controller/irq.h> #include <dt-bindings/gpio/gpio.h> / { compatible = "brcm,bcm2835"; fragment@0 { target = <&spi0>; __overlay__ { status = "okay"; }; }; fragment@1 { target = <&spidev0>; __overlay__ { status = "disabled"; }; }; fragment@2 { target = <&spidev1>; __overlay__ { status = "disabled"; }; }; fragment@3 { target = <&gpio>; __overlay__ { adis16480_pins: adis16480_pins { brcm,pins = <6 12>; // interrupt and reset brcm,function = <0 1>; // in out }; }; }; fragment@4 { target = <&spi0>; __overlay__ { /* needed to avoid dtc warning */ #address-cells = <1>; #size-cells = <0>; adis16480: adis16480@0 { reg = <0>; pinctrl-names = "default"; pinctrl-0 = <&adis16480_pins>; spi-cpha; spi-cpol; reset-gpios = <&gpio 12 GPIO_ACTIVE_LOW>; spi-max-frequency = <15000000>; /* use DIO1 as data ready by default */ interrupts = <6 IRQ_TYPE_EDGE_RISING>; interrupt-parent = <&gpio>; }; }; }; __overrides__ { device = <&adis16480>,"compatible"; drdy_dio2 = <&adis16480_pins>,"brcm,pins:0=25", <&adis16480>,"interrupts:0=25", <&adis16480>,"interrupt-names=DIO2"; drdy_dio3 = <&adis16480_pins>,"brcm,pins:0=4", <&adis16480>,"interrupts:0=4", <&adis16480>,"interrupt-names=DIO3"; drdy_dio4 = <&adis16480_pins>,"brcm,pins:0=5", <&adis16480>,"interrupts:0=5", <&adis16480>,"interrupt-names=DIO4"; }; }; |
make menuconfig
, look for module by typing ./adis16475
or ./adis16480
and setting the module with [M]
in front of their name. Save changes. arch/arm64/boot/dts/overlays/adis16475-overlay.dts \
or
arch/arm64/boot/dts/overlays/adis16480-overlay.dts \
and added to Makefile: arch/arm64/boot/dts/overlays/Makefile
the following line:
adis16475.dtbo \
or
adis16480.dtbo \
/boot/firmware/config.txt
:[all]
dtoverlay=adis164XX
dtparam=device="adi,adis16YYY-Z"
An example for adis16505-2, supported by module adis16475:
[all]
dtoverlay=adis16475
dtparam=device="adi,adis16505-2"
After reboot, the driver should be ready to use.